6/15/2021 9:19 PM | |
Joined: 9/1/2017 Last visit: 6/9/2024 Posts: 156 Rating:
|
Hi
Take a look at below link, hope it is what you are looking for: Data Exchange between S7 Station and PC Station with SIMATIC NET OPC Server Regards |
6/17/2021 10:31 PM | |
Joined: 6/4/2021 Last visit: 3/14/2022 Posts: 14 Rating:
|
Thank you for your response, this seems to help a bit. Although the biggest challenge in this would be that I don't have access to the PLC program. I would be nice if there was something that could fetch the DB tags and read them into my pc. But I will try to look into this option as well. Cheers! |
6/27/2021 8:41 AM | |
Joined: 9/1/2017 Last visit: 6/9/2024 Posts: 156 Rating:
|
Hi
Do you have related wincc (runtime) project in your pc station? You can also configure HMI device as opc server(Classic/UA).in this manual you can find more about wincc advance v14. I've tested this solution with wincc runtime v7.0 sp3 as opc da server and using cogent data hub as da tunneller . another possible solution is to use third party opc servers. hope this helps |
Last edited by: Jen_Moderator at: 06/28/2021 10:54:34Optimized link. |
|
Follow us on