12/14/2017 10:30 AM | |
Joined: 11/8/2017 Last visit: 3/30/2023 Posts: 2 Rating:
|
Hi all, We are trying to configure our RF reader with S7300 CPU. ****************************************** COMPONENTS WHICH USED ARE MDS 100 RF 240 R RF 160C M12 ,7/8 CONNECTION BLOCK ******************************************* We are using standard library given in the following application example for configuring the RFID. https://support.industry.siemens.com/cs/us/en/view/63969277 ****************************************** After configuration we are trying to reset the RF160C but its giving error ( error code : 1500). We assume that error might be the problem with the RF parameters because all the hardware is new. am using only x1 port other port (x2) is open and profibus port was terminated. is there any specific memory need to be select for if using only one reader.. what are the major parameter to be set. in RF160C (Eg. ERROR LED SUPPRESSION ,MDS ON_TIME ETC). thanks in advance REGARDS #@$# |
Last edited by: Jen_Moderator at: 12/14/2017 2:50:41 PMInserted righ links. |
|
Follow us on