Industry Online Support
Technical Forum
1/29/2008 9:37 AM | |
Joined: 5/8/2006 Last visit: 10/16/2024 Posts: 1085 Rating: (78) |
Hi, you need WinCC flexible 2005 or later, MPI or Profibus subnets andcomponents which routing capability. The flexible project have to integrated in STEP 7. The WinCCflexible Engineering Station must be connected to an MPI bus or to a PROFIBUS. The HMI device to which the project is to be transferred must also be connected to an MPI bus or to a PROFIBUS. |
Follow us on