8/9/2012 2:35 PM | |
Joined: 7/7/2010 Last visit: 8/30/2024 Posts: 15125 Rating: (2411)
|
Simple solution is to purchase the rtd temperature input module. https://support.automation.siemens.com/BR/llisapi.dll?func=cslib.csinfo&lang=en&objid=43346925&caller=view With this device, you wire your rtd per the module instructions, and if you choose the default analog input address, the actual temperature is read in your user units (C/F) directly without any computations. If you want to do it a different way and use some other method, it will be very difficult. Good luck. |
Last edited by: huggy_d1 at: 8/9/2012 2:37 PMscience guy |
|
8/9/2012 3:55 PM | |
Posts: 17 Rating: (0) |
Oh, no problem! I thought they maybe were something else. Thanks for your attention Mr Hugg1_d1. I will see what can I do. Regards! Luis |
Follow us on