5/14/2008 12:30 PM | |
Joined: 4/25/2008 Last visit: 7/8/2024 Posts: 18 Rating:
|
Hi, I am trying to communicate WinCC with CP1613 Redconnect for the last 2 days but unable to communicate. I have attached a zip file containing all the H/W config and Net Pro settings. Please can any one check the same. I also want to know the settings for WinCC for RedConnect. Thanks Attachmentimg.zip (487 Downloads) |
5/14/2008 2:47 PM | |
Joined: 9/27/2006 Last visit: 7/13/2024 Posts: 12268 Rating:
|
Hello mickey; Your attachmnent shows a PLC configuration similar to those I have done in similar projects, basically it looks good. What have you you done in the WinCC channels to use the redconnect? Maybe you have access to it already, but have a look at this FAQ, it contains a link to an application manual on fault-tolerant S7 communication via IE for WinCC. http://support.automation.siemens.com/WW/view/en/16667714 It goes through the same PLC configuration you did, but expands on what has to be done in the WinCC application. Hope this helps, Daniel Chartier |
3/12/2012 2:15 AM | |
Posts: 32 Rating:
|
Is the name of your workstation PC Station? I believe the PC station name should be the computer name of the workstation. Kindly check. |
3/18/2015 7:51 AM | |
Posts: 16 Rating:
|
Hi J_Bell, Currently my system is S7-400H redundant. The two PLC is connected to a switch (via PLC ethernet port), and a WinCC PC Station is connected to the switch via CP 1623. As u said, i need to activate the CP Mac-address, and deactivate the TCP/IP address. But how about the PLC side, do i need to activate the MAC address in PLC too? I can't find it. When i activate the CP Mac-address, and deactivate the TCP/IP address, it turn out that "No Connection could b established between..." when i compile the changes. Any idea what could cause this error. I have attached the error pic. Under Set PG/PC Interface, im using CP 1623.RFC1006.1, as shown in the attached pic. Appreciated that if u guys can help. Thanks!! AttachmentRef.rar (176 Downloads) |
Follow us on