5/31/2016 12:03 PM | |
Posts: 4 Rating: (0) |
Hello, I have been trying to get a connection between my S110 CU305 PN and a S1200 PLC via Profinet. I have imported the S110 via a GSDML file in the network and made a profinet connection between PLC and CU. Also I have used a Telegram 111 from the global library in TIA Portal. I configured the drive in Starter and added the Telegram 111 as the telegram type for my motor. The compilation and downloading to the PLC goes without problems, only a warning for the protection. When i go online in tia portal, the PLC says there is an error in the lower level component, which occurs in the profinet interface. The Sinamics s110 which is added in the distributed I/O cannot be reached. A similar problem occurs in the following link, but his solution appeared to be the order in which the telegram was read out. In the attachments you can find the pictures with the fault when I try to go online, the network configuration, telegram configuration in Starter and the installed software. The products used are as follows: power module: 6sl3210-1pe12-3al1 Servo motor: 1fk7032-2ak71-1rg0 controt unit: 6sl3040-0ja01-0aa0 PLC: Simatic S7-1200: 6es71214-1bg40-0xb0 CPU 1214c AC/DC/RLY Thank you Bert AttachmentPictures.zip (197 Downloads) |
Follow us on