5/27/2013 10:32 PM | |
Joined: 9/27/2006 Last visit: 5/7/2024 Posts: 12257 Rating: (2666) |
Hello Amol; What S7 platform are you planning to use? There are S7-300, S7-400, S7-1200 CPUs, each with there own specific modules that you can select. As an exercise, i have attached exracts from the following manual, in which you will find technical information on the proposed modules. You will see that the electrical specs of these digital modules fall quite close to those of the S5 modules you are trying to replace (except that the DI module is a 16-point DI, of course). SIMATIC S7-300 S7-300 Module data Have a look, and tell us if you plan to use another platform. Information is easy to find on the Siemens Support site, and members of this forum have a good reputation for helping. Hope this helps, Daniel Chartier |
Last edited by: O_Moderator at: 5/28/2013 8:10 AM |
|
5/28/2013 4:38 PM | |
Posts: 9 Rating: (0) |
Dear Sir Thanks For Your Reply I want Convert In S5 System in S7-300 Platform.I have Search With Datasheet of Conversion Of S5 TO S7 Hardware As attached But IN this Datasheet Both DI & DO Module not Available. In Description Of S5 Module It Showing That Interrupt & Manual For Same Not Getting Anywhere Please Suggest Me S7-300 Compatible Module For Above S5 Module. Attachment5_SIMATIC_S5_S7_renewal_manual_en.pdf (417 Downloads) |
6/1/2013 5:46 PM | |
Posts: 9 Rating: (0) |
Dear Sir As I check On Siemens Website https://eb.automation.siemens.com/mall/en/in/Catalog/Product/6ES5434-7LA11 Showing That Module6ES5434-7LA12 isSuccessor of6ES5434-7LA11& Another Attached Siemens Compatible Module Datasheet Is Shows on Page No:16 ShowingCompatible Module Is 6ES7-321-1CH00- 0AA0 FOR6ES5434-7LA12.Can I used this Module (6ES7-321-1CH00- 0AA0) For S5 Module of MLFB6ES5434-7LA11? Attachment1_Adapter_Eng_V3_0.pdf (133 Downloads) |
6/1/2013 10:05 PM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (836) |
Hello, Please see in the end of the following file, which S7 modules are equivalent to which S5.
|
Ayman Elotaify |
|
6/2/2013 10:06 AM | |
Posts: 9 Rating: (0) |
Dear Sir Thank For Your Reply But6ES5-434-7LA11 &6ES5-441-7LA11 For This Two Module Compliable S7 Module Not Avaliable In that Sheet.
|
Follow us on