11/21/2011 4:15 PM | |
Posts: 5225 Rating:
|
Marko Bursic, I can not help but wonder if your 1st instinct was not right. -------- tigger := not trigger distance := abs_position_ask - abs_position_read if trigger == 1 then MC_MoveRelative(distance) //alternating trigger if trigger == 0 then MC_MoveRelative(distance) --------- The position as <Axis name>.MotionStatus.Position is not important. It can however be kept up to date by doing direct active homing. The automatic software limits should be disabled though and be writen in code instead. Would this simple method not work? |
11/21/2011 6:04 PM | |
Posts: 5225 Rating:
|
There is something we overlooked - if we do use the trajectory planner. In this MATH EXPLAINED LINK the trajectory is not what we use in S7-1200. Setting up motion in the S7-1200, there is a minimum speed to reach.. not zero as in the trajectory math as above. See the JPG for a picture view of the difference. The math function will have to be rewritten or the minimum speed should be very low. ::UPDATE:: Did not see previous posting before posting this note. Will answer previous post soon. |
Last edited by: William B. at: 11/21/2011 6:07 PMupdate note |
|
Follow us on