12/4/2017 12:57 PM | |
Posts: 1 Rating: (0) |
Hi All - This is my first post on the Support system and I'm a completely new to DP-DP slave communication. I have a new S7-1200 CPU fitted with a CM 1242-5 comms module that I am trying to interface via profibus with my master system which is a CPU 417-4 programmed in Step 7. l have added the CP-1242-5 module to the master HW profibus configuration in step 7 as a Profibus Slave however I'm unsure how to set up the Input/Output communication to match the data addresses of the Comms Module. Do the Addresses of the Input / Output Byte and Word modules that need to be dragged into the CM1242-5 config need to match the slave addresses allocated on the s7-1200 side?? i.e - If a digital output from the S7-1200 is addressed as Q500.0 at the DP slave (CM 1242-5) - does it need to be addressed as I500.0 at the CM 1242-5 adddressing in the main project HW configuration? I hope this makes enough sense for someone to assist? Thank you all for any help on this. John Higg ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/4/2017 2:46:17 PMNew subject after splitting |
|
Follow us on