9/20/2011 3:03 PM | |
Joined: 1/17/2007 Last visit: 7/29/2024 Posts: 1544 Rating:
|
Is data traffic being seen between the client and server? (use wireshark to check this). Is it just the data that is incorrect? The fact that you have no error code would suggest that the communications is working. It might be that the data is not correct or that you are requesting the wrong registers in the PAC. The address you are using (30001) and data length will try to read the first 10 "Input Registers" in the PAC. It is very difficult to say what the issue is without further information (a wireshark capture will help here). |
Programming today is the race between software engineers building bigger and better idiot proof programs, and the universe producing bigger and better idiots. |
|
9/20/2011 10:43 PM | |
Joined: 7/7/2010 Last visit: 8/15/2024 Posts: 15090 Rating:
|
That's good news! |
science guy |
|
9/27/2012 4:36 PM | |
Posts: 2 Rating:
|
thomas,I have the same configuration, but it won't run. Can you send me you application or help me out? Thanks in advance. |
9/27/2012 5:06 PM | |
Posts: 3093 Rating:
|
Hello Rolf, which error do you get? Regards, Kaulquappe |
Follow us on