11/14/2023 10:13 AM | |
Joined: 3/11/2019 Last visit: 6/14/2024 Posts: 1476 Rating: (266) |
Hi, MLFB 6AG1500-0HP00-4AB0 is a "bundle" with different parts. How do you configure a SIPLUS extreme component with the TIA Portal?Check for the ET200SP accordingly. regards sancruz |
Last edited by: sancruz at: 11/14/2023 10:14:06Feedback appreciated, please rate |
|
1/8/2024 6:46 AM | |
Joined: 11/28/2019 Last visit: 4/16/2024 Posts: 6 Rating: (0) |
Hello, we are configuring 6AG1155-6AU00-7HM0 part number in tia portal v18 unified edition, but in this part number not available in hardware list, also we using DI/DO (6AG1131-6BH01-7BA0) siplus module, that also available. Please suggest the solution as soon as possible. |
1/8/2024 7:37 AM | |
Joined: 3/11/2019 Last visit: 6/14/2024 Posts: 1476 Rating: (266) |
Hi,
A possible solution is already available in the FAQ above.... Is the product number of the SIPLUS variant not available in hw catalog, the standard product number of which the product is based on can be used. In addition to that. The answers from other users are based on a voluntary basis in addition to their regular work. -> US ET 200SP IM155-6PN R1 based on 6ES7155-6AU00-0HM0 6AG1131-6BH01-7BA0-> SIPLUS ET 200SP DI 16x24VDC Standard based on 6ES7131-6BH01-0BA0 regards sancruz |
Last edited by: sancruz at: 01/08/2024 07:39:40Last edited by: sancruz at: 01/08/2024 07:41:56Feedback appreciated, please rate |
|
Follow us on