6/25/2024 11:33 AM | |
Joined: 5/29/2024 Last visit: 7/12/2024 Posts: 29 Rating: (3) |
Hi raj_srk! The ET200S range is already in the discontinuation phase announcement: -> Update announcement of product phase-out for ET 200S components (status Decembert 2023) https://support.industry.siemens.com/cs/ww/en/view/109767411 Therefore, it is advisable to purchase the modules of an ET200SP. In the FAQ comes the Excel with the equivalents. If I had that ET model that is indicated in the post, there would be no problem using it. |
Last edited by: The Helping Hand at: 06/25/2024 14:03:45Link optimized If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on