4/28/2012 8:50 AM | |
Posts: 20 Rating: (0) |
Hi I am using a CPU-315 2 PN/DP I want to Read out the error diagnostics information. is it possible? if it is then is there any sample program to do so? Regards. |
4/28/2012 9:10 AM | |
Posts: 947 Rating: (45) |
See help on sfc51. On sypport can find samples. See also "Report system error" in Hw-config |
4/28/2012 10:54 AM | |
Posts: 153 Rating: (2) |
have a look on attached pdf regarding step 7 error codes
AttachmentSTEP7_ErrorCode_engl.pdf (1398 Downloads) |
This contribution was helpful to2 thankful Users |
4/29/2012 6:57 PM | |
Posts: 947 Rating: (45) |
if you use the system generated error messages ( "Report system error" ), then will be generated OB, which transmit error controller message in WinCC |
Follow us on