8/4/2010 7:43 AM | |
Joined: 3/21/2006 Last visit: 10/7/2024 Posts: 10229 Rating: (1181) |
Hello, Look at Connection of Masterdrives to Profibus-DP. Best regards, Hristo Mihalev |
8/4/2010 1:15 PM | |||
Joined: 3/21/2006 Last visit: 10/7/2024 Posts: 10229 Rating: (1181)
|
1. Hardware conection between drives and CPU is using profibus connectors and cable. 1.1 Connectors - Product Information on PROFIBUS-bus connector with/without PG socket to 12 MBaud 1.2 Cable -
Write in google "profibus cable" and you'll see a lot.... http://www.maser.com.au/au/ProfibusProductBulletin.pdf More info about Profibus you could find at http://support.automation.siemens.com/WW/view/en/1971286 For the moment leave DRIVE ES Basic software. Work with Step7 and DriveMonitor.(Current DriveMonitor Version V5.4 SP2 for SIMOVERT MASTERDRIVES, MICROMASTER and SIMOREG.). USB/MPI is for CPU programming. It's not "connected" with profibus connection between drive and CPU. Be careful with cables - don't plug each cable in to "matched" hole. Best regards, Hristo Mihalev |
||
8/4/2010 2:48 PM | |
Joined: 3/21/2006 Last visit: 10/7/2024 Posts: 10229 Rating: (1181)
|
You could use integrated I/O in CPU and with them to control drive&motor. Look at SIMOVERT MASTERDRIVES Motion Control Compendium (MC 2.4) how to connect them. Best regards, Hristo Mihalev |
8/4/2010 9:33 PM | |
Posts: 13 Rating: (0) |
Dear friends, Thanks for your help and interest. I will study as you said . Best Regards. Kaan ALPER |
This contribution was helpful to1 thankful Users |
Follow us on