5/17/2006 9:51 PM | |
Posts: 4 Rating:
|
Hello Dang, I think that you must update your Firmware Gr Semi |
5/20/2006 6:15 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating:
|
Hi Dang, What version is the H-CPU and which CPU is it, the newest? (6ES7414..... ) If you have a Diagnostic Buffer of the CPUs when this is happening then it is usefull to find the problem. [;)] Are you using Failsafe as well, that because you have to type ina password? If all the LEDs are flashing then the CPU have found a command where no code for is, they call it the "Defect" state. [8)] When there is a Firmware update necessary, then you have to download the firmware from the next link: http://support.automation.siemens.com/WW/view/en/6741018 Requirements for creating the operating system update card:
I hope you have enough information to get your system running well.... [:o] |
Last edited by: Late at: 5/20/2006 6:24 PMAnswers on the extra Questions put also in the answer.... I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on