9/29/2019 5:53 PM | |
Joined: 5/25/2015 Last visit: 5/11/2023 Posts: 44 Rating: (1) |
Hello all, I want to setup Fault Tolerant communication between 2 Nos of S7 400H over Profinet . I have searched this forum and till now i only found this related link. I dont want to use Get Put communication here as it wont give me error on passive partner. Can you provide any application program , getting started manual for such cases. Also if i use AG_SEND & AG_RECEIVE, which CP Hardware address should i put for L_ADDR ( Hardware identifier) as this is going to be redundant comm . Active Partner : CPU 417-5H PN/DP 6ES7 417-5HT06-0AB0 CP 443-1 6GK7 443-1EX30-0XE0 Passive Partner : CPU 417-5H PN/DP 6ES7 414-4HM14-0AB0 CP 443-1 6GK7 443-1EX20-0XE0 |
9/30/2019 1:40 PM | |
Joined: 8/21/2014 Last visit: 7/12/2024 Posts: 994 Rating: (13) |
Closed because question was posted twice. Please use: S7 400H Fault Tolerant Communication in the SIMATIC S7-400 / S7-400H / S7-400F /FH conference. |
My Forum is the place to personalize your profile, |
|
Follow us on