Industry Online Support
Technical Forum
10/11/2009 5:01 PM | |
Joined: 7/2/2008 Last visit: 5/29/2024 Posts: 928 Rating: (306) |
Hello DesignTech, You are not missing anything, Y-Link is constructedof 2 IM153-2 (ET200M) and a Y-Coupler and they are linked together by active bus units. If one IM153-2 fails, the H-System can still communicate with slaves using the other IM but if Y-Coupler or both IMs fail then you will lose all stations. It is always better to go for red. bundlesThen, 1- Each ET200M station will not depend on Y-Link status 2- You will ignore the bottle neck of Y-Link (244 bytes of I/Os). 3- You can make use of DPV1 interrupts but behind Y-Link youwill use DPV0 ET200M. Best regards. H-H |
Follow us on