12/15/2008 7:18 AM | |
Posts: 12 Rating: (0) |
hi we are having s7-400 cpu 412-2 DP in software redundancy, we are using the Im153-2 6ES7153-2BA020-0AB0 with active bus module for et200m and digital io's. we are having CP443-1. we are using mpi as software redundancy problem both are acting as master. redundant soft link failed bit is setting. but we checked cable and its found ok. attached is the file i have seen the thread of software redudancy in forum. but could u not able to find solution would u pls help regards dilipan AttachmentSTATION_A.zip (240 Downloads) |
12/15/2008 7:21 AM | |
Posts: 12 Rating: (0) |
Program attachment 1
AttachmentTesting.zip (245 Downloads) |
12/15/2008 7:29 AM | |
Posts: 12 Rating: (0) |
program attachment 2 rename the file to Testing.zip.z01 AttachmentTesting.z01.zip (227 Downloads) |
12/15/2008 7:31 AM | |
Posts: 12 Rating: (0) |
program attachment 3 rename the file to Testing.zip.z02 AttachmentTesting.z02.zip (234 Downloads) |
Follow us on