4/21/2020 8:14 PM | |
Joined: 1/22/2014 Last visit: 5/21/2024 Posts: 32 Rating:
|
Hello, May I open this old topic, I have read several topics and manuals but do not find a working answer. The S7 Communication between the S7-1500 and a S7-400 CP 443-1 Card is not established. The S7-1500 is the active element, with TSAP 10.01. The CP 443-1 is the “Unknown” partner where I put TSAP 11.05. (05 because the CP 443-1 is at the 5 slot on the S7-400 rack, I tried also with 03 the CPU slot). The S7 Subnet ID in the S7-1500 is the same as in the S7-400 CP 443-1. Normally in the S7-400 or CP 443-1 I do not to do anything, only configuring at the S7-1500 side. Put/Get in the S7-1500 are authorized, DBs in both CPU are the same, network is OK… but no S7 Connection. Is there something what I missed ? Thanks in advance ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/22/2020 10:35:02New subject after splitting |
|
3/30/2021 6:15 PM | |
Joined: 4/8/2019 Last visit: 7/9/2024 Posts: 1 Rating:
|
Hello All Any new news, i am facing the same. |
Follow us on