7/11/2021 8:59 PM | |
Posts: 15 Rating:
|
What is the difference between s7 connection and open user communication? Also, I want to know if the s7 connection works on Profibus master - salve |
7/11/2021 9:54 PM | |
Joined: 3/30/2020 Last visit: 7/17/2024 Posts: 4628 Rating:
|
S7-communication is a generic name for a protocol between Siemens devices. This could be used on PPI / MPI / Profibus / Profinet. The PLC instruction pair that is most associated with S7-communication is PUT and GET, but it the protocol is much wider than this. Open User Communication (OUC) is Ethernet based which includes TCP and UDP variants. It is not bound to Siemens products. In the PC programming you can look to 'socket' programming to create a partner. On the OUC theme there is a library that is worth a look: Best health. |
Last edited by: qwazee at: 07/11/2021 21:56:56Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to
2 thankful Users |
Follow us on