Industry Online Support
Technical Forum
12/1/2014 6:40 AM | |
Posts: 21 Rating: (0) |
Hey William B I'm having the same problem that i'm working on a recipe but its not the kind of recipes mentioned in TIA Portal and s71200 manuals, its a bit more complicated . As mentioned in the start of this thread , i also have 5 tasks and there are 3-4 parameters in each task, these tasks are performed in different order in every recipe and these tasks are repeated in each recipe about 3-4 times (with different parameter value) , i also tried to do this with the help of DB but couldn't handle all that in one PLC prog. Also i need to code in a manner that the operator can also make a recipe by picking up tasks in any order with different parameters through a HMI. How do i do it??? Kindly help me out in this Thanks and Best Regards,
------------- new subject after Splitting from Save values of Data block in Different data Blocks Using Hmi Ktp600 |
Last edited by: CS Moderator at: 12/2/2014 10:05 AMsplitting Last edited by: Paras at: 12/1/2014 6:42 AMLast edited by: Paras at: 12/1/2014 6:40 AM |
|
12/1/2014 5:00 PM | |
Posts: 5225 Rating: (1193) |
Question posted by Paras, continues in its own thread at [LINK]. |
12/2/2014 10:08 AM | |
Joined: 9/1/2005 Last visit: 10/14/2024 Posts: 4109 Rating: (195) |
closed cause question posted twice. The second thread with the subject Working with Recipes [S7-1200 (1214) & KTP 600 ]is published within the same conference. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on