Industry Online Support
Technical Forum
10/27/2011 10:41 AM | |
Joined: 7/2/2008 Last visit: 9/30/2024 Posts: 928 Rating: (308)
|
Hellonandgate,
You can read the following inAutomation System S7-400 Hardware and Installation
If your card is FLASH card then you have 2 ways, 1- Download directly to the memory card before insertion by a PG or prommer. Or 2- Insert the memory card in the CPU and in SIMATIC Manager go to PLC> Download user program to memory card. If the memory card is RAM type then you have to insert first and downlaod. Best regards. H-H |
Follow us on