8/13/2013 1:03 AM | |
Joined: 9/27/2006 Last visit: 10/17/2024 Posts: 12289 Rating: (2687)
|
Hello saeed; Based on point 3 of the following FAQ: Which cables can you use for connecting the PC and the TS adapter? you cannot use a USB to serial cable to extend the PC adapter to a USB port: The following connections are not possible with a PC or USB adapter:
Hope this helps, Daniel Chartier |
8/13/2013 6:10 AM | |
Posts: 262 Rating: (45) |
Hi, Hope this old post will help .. |
8/13/2013 6:14 PM | |
Posts: 7 Rating: (0) |
thanks a lot . but The problem was not resolved. |
8/15/2013 11:03 AM | |
Joined: 9/1/2005 Last visit: 10/14/2024 Posts: 4109 Rating: (195) |
Follow up question published by daadis split to a seperate thread with the subject apply supply(24V) at pin 7 of parallel serial converter Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
8/27/2013 4:28 PM | |
Posts: 376 Rating: (57)
|
Hello saeed, I think you already have invested much time and the problem is not solved. Here an alternative to your hardware configuration. Please open this Link: http://support.automation.siemens.com/WW/view/en/62195483 or http://support.automation.siemens.com/WW/view/en/62195483/td Best regards Azteke0110 |
Last edited by: Azteke0110 at: 8/29/2013 8:35 AM |
|
8/28/2013 5:59 PM | |
Joined: 10/31/2011 Last visit: 9/2/2024 Posts: 400 Rating: (5) |
Plz recheck your target link |
This contribution was helpful to1 thankful Users |
Follow us on