12/15/2021 10:07 PM | |
Posts: 257 Rating: (75)
|
Hello SIOS Forum Community. With the new CPU S7-1518HFS7-1518HF, a highly available S7-1500 CPU with integrated safety functionality is available for the first time. This CPU combines the established safety function of the S7-1500F CPUs with the high availability of an S7-1500H (previously the S7-1517H). The deployment of the S7-1518HF CPU requires STEP7 V17. For the other redundant S7-1500 controllers (1513R, 1515R, 1517H), it is still possible to realise fault security via an additional F-CPU. There are various options for coupling this F-CPU to the S7-1500R/H:
Best regards, SIMATIC International Technical Support Hub |
Follow us on