3/4/2010 5:15 PM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936) |
Since there is a very little chance you deleted them, I guess your using: File->Open projects->Sample projects to search for the color_gs example. But the color_gs project is archived, so in order to use, you have to use the"RETRIEVE" button. So click on the RETRIEVE button in Simaticand search in the folder: C:\Program files\Siemens\Step7\Examples_MP. Theexamples are there.... |
If I could help you, you can use the RATE button. Thank you. |
|
3/4/2010 6:24 PM | |
Joined: 11/15/2009 Last visit: 8/16/2024 Posts: 380 Rating: (47) |
Sorry fe11x! Attached is a extraction from manual (PCS 7 DVD\_Manuals\English)“Process Control System PCS 7Getting Started – Part 110.1.1 How to Open the Example Project” Regards AttachmentHow to open the Example Project.pdf (754 Downloads) |
3/4/2010 6:36 PM | |
Joined: 11/15/2009 Last visit: 8/16/2024 Posts: 380 Rating: (47) |
Not folder Examples but C:\Program files\Siemens\Step7\Examples_MP |
3/4/2010 7:05 PM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936) |
you have illegal version or what? |
If I could help you, you can use the RATE button. Thank you. |
|
3/4/2010 8:01 PM | |
Posts: 10 Rating: (0) |
not illegal, it is in my cement plant computer... |
Follow us on