10/25/2013 8:08 AM | |
Joined: 10/3/2010 Last visit: 9/30/2024 Posts: 1562 Rating: (192) |
Do you have layers in those pictures which are default hidden? This symptom is most commonly caused if you have hidden layers in your picture. Whenever you open the picture in Graphic Designer, it checks which layers were set as hidden and performs this action again. This is seen by WinCC as a picture change each time and that's why you get this prompt. |
B r g d s , |
|
10/25/2013 2:41 PM | |
Joined: 9/7/2005 Last visit: 11/7/2023 Posts: 31 Rating: (9) |
Seems the issue was fixed in WinCC 7.2 Update 2 (http://support.automation.siemens.com/WW/view/en/78537522) Readme file: 2.1 Improvements and changes compared to WinCC V7.2 ... WinCC Basic ... • Graphics Designer: ... - When an unchanged process picture is closed, you are not prompted to save the picture Update 3 is also relased. Regards, Tolleif |
Siemens Oil&Gas Offshore |
|
10/25/2013 8:08 PM | |
Joined: 10/3/2010 Last visit: 9/30/2024 Posts: 1562 Rating: (192) |
Just tried what Tolleif replied above for V7.2.0.3. This issue is indeed solved. So, depending on your version, you have a fix or not. |
B r g d s , |
|
This contribution was helpful to1 thankful Users |
10/28/2013 4:23 PM | |
Posts: 15 Rating: (0) |
That has fixed it. I am on v7.0. I showed all layers and now the issue is resolved. Many thanks. |
7/21/2015 9:43 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4766 Rating: (122) |
|
Follow us on