7/6/2023 9:49 AM | |
Joined: 1/21/2013 Last visit: 8/4/2024 Posts: 3044 Rating:
|
Hi robbie c, In my opinion, such a structure should work. You should first check if the ET 200SP motor modules fit your conveyor motors. You should also consider the need for fail-safe modules instead of standard modules. If you are already using ET 200SP and it is a simple application, you might also consider the CPU 1510SP-1 PN (or CPU1510SP F-1 PN). You can use this CPU instead of an ET 200SP interface module, which will reduce the cost. Did you know that the Siemens TIA Selection Tool is a free tool for planning your application? Kind regards |
Follow us on