10/28/2018 7:45 AM | |
Joined: 12/18/2014 Last visit: 7/15/2024 Posts: 33345 Rating:
|
Service Pack 1 for STEP 7 V5.6 / Service Release 1 for STEP 7 Professional 2017 What's New in STEP 7, Version 5.6? The following subject areas have been updated: Operating systems ·The operating systems MS Windows 10 Pro and Enterprise MS Windows Server 2012 and MS Windows Server 2016 are supported as of STEP 7 V5.6. You can find more detailed information on this in the accompanying file "Readme.rtf". Configuring and Diagnosing Hardware ·As of STEP 7 V5.6, you can update the firmware for CPUs 410 as of V8.2 in two separate steps. You can find more detailed information on this under "Online Update of the Firmware for Modules". ·As of STEP 7 V5.6 SP1, the GSDML schema 2.35 is supported. System Diagnostics ·As of STEP 7 V5.6, you can read out security events for CPU 410-5H as of firmware version V8.2 and save them on your PG/PC via the "Save Security Events" dialog box. ·In STEP 7 V5.6, the "Process Objects" tab of the module status is renamed to "SEC" (SEC means System Expansion Card.), and further properties are dsplayed for the license status. SIMATIC Manager ·As of STEP 7 V5.6, the number of selected objects is shown in the status bar. Checking Block Consistency ·As of STEP 7 V5.6, you can perform an extended consistency check with symbolic addressing. You can find more detailed information on this in the help for block consistency under the entry "Extended consistency check". |
This contribution was helpful to
2 thankful Users |
10/28/2018 11:43 AM | |
Joined: 11/16/2006 Last visit: 3/1/2024 Posts: 92 Rating:
|
old MS Windows 7 SP1 x64 are supported :) |
Follow us on