12/26/2013 5:28 PM | |
Posts: 8946 Rating: (999) |
May be, the tag is overwritten inside PLC? |
12/27/2013 8:18 PM | |
Joined: 11/8/2011 Last visit: 7/2/2024 Posts: 387 Rating: (43) |
no tag is no where overwritten as i am using instance db |
12/30/2013 11:33 AM | |
Joined: 11/8/2011 Last visit: 7/2/2024 Posts: 387 Rating: (43) |
Thanks for the reply it works fine for set function and reset function separate but it not matches the requirement |
12/31/2013 9:02 AM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating: (1166) |
Hello SGp, Are you using the latest TIA Portal version? Perhaps you can download Service Pack 1 for TIA Portal V12 Service Pack 1 for SIMATIC STEP 7 V12 (TIA Portal) incl. PLCSIM Service Pack 1 for SIMATIC WinCC V12 (TIA Portal) And the latest update Updates for STEP 7 V12 SP1 and WinCC V12 SP1 Best regards, Wizard |
This contribution was helpful to2 thankful Users |
1/4/2014 1:11 PM | |
Joined: 11/8/2011 Last visit: 7/2/2024 Posts: 387 Rating: (43) |
HI experts, still its not working with v12 sp1, same problem exist with V12 Sp1 Please guide me on this Thanks in advance |
Follow us on