11/21/2014 12:50 PM | |
Joined: 11/29/2011 Last visit: 5/20/2024 Posts: 1358 Rating: (231) |
Hi, I have a question about copy a structure embended into a UDT. I need to define a UDT as an IN_OUT parameter. One structure of this UDT needs to be copied into a structure in Static area(.TX part). The other Structure of the UDT needs to be written from its match in the Static area(.RX part). The 2 structures in the Static area will need to work with SFC14/SFC15. I tried to SFC20 to do the copy job into/from the static area, but it seems not like the DOT in the source and destinamtion input. Is there any easy way around this problem? I attached the UDT in ziped text file. Best Regards:
AttachmentUDT320.zip (41 Downloads) |
Last edited by: MicroMan at: 11/21/2014 12:54 PMAttachment. - What you read here, please check with manuals and your requirements. |
|
Follow us on