1/13/2023 7:22 AM | |
Joined: 8/3/2009 Last visit: 10/10/2024 Posts: 13897 Rating: (1756)
|
Hello Hakan1122 yes if you use a graphic in a WinCC Basic/Comfort/Advanced project then it is "compiled into" the runtime files and has to be there in engineering. the only way would be to work with html-browser control. here you can have access to external data. (as already suggested) -> FTP is also a problem because there is no automatic function to work with the panel as FTP Client. you only can try to integrate the panel into the network and have access to a network share: https://support.industry.siemens.com/cs/ww/en/view/92346478 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on