9/26/2024 1:39 PM | |
Joined: 9/26/2024 Last visit: 10/1/2024 Posts: 1 Rating: (0) |
Hi everyone, I am in the middle of a project in which I need to connect an edge device (catalogue attached) with SICAM A8000, CP-8021. The edge device will run on either windows 10 or 11 and will be running a Video analytics code written in Python. Is it possible for the edge device to communicate with CP-8021 and share outputs from the Python program using Modbus RTU protocol. Thanks, Kushagra AttachmentNuvo-9531 DATASHEET.pdf (257 Downloads) |
Follow us on