Industry Online Support
Technical Forum
3/29/2010 3:54 PM | |
Joined: 10/9/2007 Last visit: 12/20/2024 Posts: 1252 Rating: (115) |
Hi Jasner Sicam SAS (the controller) and Sicam WinCC (HMI for Sicam SAS based on WinCC) are old systems and were substituted by Sicam PAS. Sicam SAS used M7 CPU, MCP card (for IEC and DNP protocols), special AI, DI, CO (command output) with 1ms resolution and 2,5kV isolation, and could also used normal IO cards from S7 world, as some communication cards from S7 (CP443-5 Basic, CP443-1). Sicam PAS is a computer-based energy automation system. If you need a RTU solution, we have Sicam 1703. More info under http://www.sicam.de/index_e.htm Mike J |
Energy Automation products: Sicam, Siprotec, Digsi |
|
12/12/2014 1:58 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4766 Rating: (122) |
|
Follow us on