Industry Online Support
Technical Forum
11/3/2014 7:05 AM | |
Posts: 11 Rating: (0) |
Dear All, In one of the plant we have Siclock TC 400 , and we want to configure it as it will get external synchronisation from NTP server having IP address 10.1.1.30 ( GPS IP ) , Customer has provided me the ethernet cable from there CP card where i am getting ping of the above IP address. Now I am not able to get synchronized time in our siclock , kindly help me what parameter need to be configured in siclock , how to check that i am receiving clock signal from NTP server Please help --------------------------- New subject after splitting from How do you synchronize the date and time between an PC and an S7-300/S7-400 controller with WinCC ? |
Last edited by: Min_Moderator at: 11/3/2014 2:45 PMSplitted |
|
11/4/2014 10:39 AM | |
Posts: 457 Rating: (46) |
Hello, if you connect LAN (NTP service) to Siclock then the LED Link/active shows connection. Time will be showed in the display. See chapter 8.1 of Operating instructions. You can use configuration tool for setup. Use only one IP/subnet, do not define all IP-addresses as the same (see 8.2.2 Parameter list). See 9.1.2 for NTP operation. If not available: http://w3.siemens.com/mcms/topics/en/siplus/old-timesynchronisation/Documents/operating_instructions_SICLOCK_TC400_en.pdf Georg |
Follow us on