8/11/2024 8:47 PM | |
Joined: 6/4/2008 Last visit: 10/4/2024 Posts: 1497 Rating: (324) |
Hi, you don't mention if you are controlling these by PLC or digital, but I will assume digital, otherwise the question makes no sense. There are free function blocks available, if you look in the MANUAL, there are three ON-Delay timer blocks available (See section 8.3.14.14) that you can trigger to do various things with i.e. switch in a different setpoint RPM after x minutes, using the numerical switch blocks also available (see section 8.3.14.17) Regards, Graeme |
Follow us on