7/15/2024 2:54 PM | |
Joined: 5/6/2022 Last visit: 8/13/2024 Posts: 439 Rating:
|
Hi aamirawan91, Question 1: The IPC is a computer for assembly in industrial installations characterized by its robustness. What is installed in the IPC can be any client's own application, the implementation of an OPC UA / DA server, the execution of an Advanced runtime, etc. It cannot be known except by seeing the installed software. Question 2: in the case of an IPC it works the same as a standard PC. If it fails, and it is the same model and the hard drive is not corrupted, you can change from one to the other. Or if you have a backup of one PC, you can install it on another one with the same reference. Best regards!
|
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on