10/15/2013 11:42 AM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
New question splitted to Problem with Simatic PDM v8.0 Best regards O_Moderator |
6/4/2020 5:23 PM | |
Joined: 10/16/2019 Last visit: 2/23/2024 Posts: 2 Rating: (0) |
I don't know a bit about the subject. Could someone tell me the step by step to correct the error. Thank you.
|
6/4/2020 6:54 PM | |
Joined: 9/27/2006 Last visit: 5/25/2024 Posts: 12257 Rating: (2668) |
Hello alan; Welcome to the forum. Please read your question once more before we continue. You do realize that with the information provided we have little idea of what your problem is, or how we can help you? Start by telling us what version of PDM you are working with, the type of license you have for PDM and the Windows OS installed on your PC. Then describe your problem clearly, with screenshots of your error messages when you have them. Here is a link to the latest version of the PDM Device Library (for PDM v9.1), it includes a list of the integrated devices you can setup on this version of PDM. There are descriptives of the Device Library for other versions of PDM in Product Support. Check that the module you want to use is in the library. Information on the "SIMATIC PDM Device Library 1#2019" https://support.industry.siemens.com/cs/ww/en/view/109774082 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 06/04/2020 18:56:08 |
|
6/4/2020 8:40 PM | |
Joined: 10/16/2019 Last visit: 2/23/2024 Posts: 2 Rating: (0) |
Hi dchartier, The version of SIMATIC PDM is V6.0 SP5. The Windows OS is Windows Server 2003. The problem is that I can't open SIMATIC PDM, I have a kind of error. Appears "Device description could not be loaded. Please install it in the SIMATIC Manager using 'SIMATIC PDM Manage Device Catalog' or reinstall SIMATIC PDM." Could you help me.
|
6/4/2020 9:41 PM | |
Joined: 9/27/2006 Last visit: 5/25/2024 Posts: 12257 Rating: (2668) |
Hello Alan; Thank you for the information. This document is a Released for Delivery note for the PDM Device Library for v6.0 +SP5, and it has information that might be pertinent to your problem. See the screenshot below. SIMATIC PDM V6.0 + SP5 Released for Delivery https://support.industry.siemens.com/cs/gt/en/view/35125626 One more question: are you integrating your PDM software in Step 7 or PCS 7? If so, what version of Step 7, which license do you have installed your PDM software, how many tags have you selected (single-tag, 128 tags...), did you select an integration option in Step 7 or in PCS 7 ... Look at the contents of this description of PDM v6.0 as a guide: https://support.industry.siemens.com/cs/gt/en/view/21005263 I have a feeling that your error message comes from a licensing problem for your PDM installation, either the selection of licenses is incomplete for what you want to use it for, or it is installed on the wrong OS for the type of license required. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 06/04/2020 21:45:51 |
|
Follow us on