4/9/2023 7:54 PM | |
Joined: 8/3/2021 Last visit: 7/8/2024 Posts: 3 Rating:
|
hi i have the same problem when i try to use hwcnexport i always get the same error message. It says "TIA version not supported or TIA Openness is not installd" I have version v16 on TIA portal, v11 on SIMIT and v4.0 SP1 PLCsim Advanced. I also added my user in TIA Openness but it still doesn't work ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/11/2023 09:16:15New subject after splitting |
|
4/11/2023 10:27 AM | |
Joined: 5/6/2022 Last visit: 7/24/2024 Posts: 434 Rating:
|
Hi seneden, What exact versions do you have (TIA Portal, SIMIT...)? With my installation, TIA v16 Upd5 and SIMIT v11.0 Hf1, the import runs smoothly. has the Openness interface also been upgraded to TIA V16 Upd5? This is absolutely necessary for the import into SIMIT. Best regards. |
If this Information really helps, you could use the Rate function |
|
6/20/2023 11:58 AM | |
Joined: 5/11/2023 Last visit: 8/1/2023 Posts: 2 Rating:
|
Okay. I'm new to this. So where can I find that and upgrade that "Tia openness"? |
Follow us on