11/30/2009 9:26 AM | |
Posts: 160 Rating: (16) |
Hi, All this is possible you will just need to configure the relevant parameters and select the control station by using fixed levels. |
11/30/2009 9:27 AM | |
Posts: 262 Rating: (45) |
HI, Cud you please send the screen shot of Software ... and make us understand wht r u doing. pls check the control station commands to be selected whn u r not using PLC. for any fault you have to reset simocode pro and u can define the cooling down period also. AttachmentMicrosoft PowerPoint - Presentation1.pdf (292 Downloads) |
11/30/2009 11:23 AM | |
Posts: 5 Rating: (0) |
Thanks for your replies. Attached is a snapshot of graphic editor. I've selected Local2 for control station only (S1=fixed level '0' and S2=fixed level '1'). |
12/2/2009 4:08 PM | |
Posts: 5 Rating: (0) |
Thanks Valli! |
Follow us on