6/30/2009 12:34 PM | |
Posts: 5 Rating: (1) |
Everytime the drive go in operating mode appear the current fault warning W5001 power unit chip over temperature. I think that this is just only noise of signal because if I check the parameter signal r37.1 with the trace (attacced starter trace) I can se the temperature start from 30°C to over 120 °C in just only 0,7 seconds and after go down. This is not possible really!! The ambient temperature is 30°C and the cooling fan is working. Can the p290have some influence? All sinamics drives in this plant have the same kind of problem.
Thanks Attachmentwarning 5001.zip (422 Downloads) |
Last edited by: Simone-EDM at: 6/30/2009 12:38 PM |
|
6/30/2009 12:47 PM | |
Posts: 5 Rating: (1) |
the issue is possibile see on parameter r37.1 |
7/1/2009 3:47 PM | |
Joined: 9/18/2006 Last visit: 11/14/2024 Posts: 593 Rating: (64) |
Hi. Excuse me, but I have not understood *.trc Best regards. |
7/17/2009 2:48 PM | |
Posts: 5 Rating: (1) |
I'm using SINAMICS S120 CM 6SL3720-1TG37-4AA0-Z |
Follow us on