6/19/2024 8:29 PM | |
Joined: 7/17/2019 Last visit: 7/8/2024 Posts: 9 Rating:
|
Hi, Sorry for jumping on an old post, has anyone used SINAMICS G: Load sharing for two coupled drives Only i have 3 Axis that are coupled, its not a solid mechanical coupling its coupled through the product . I looked at LLoadBalance but my mechanics dont suit. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 06/20/2024 10:02:32New subject after splitting Thanks, |
|
6/20/2024 11:58 AM | |
Joined: 10/11/2006 Last visit: 7/12/2024 Posts: 5874 Rating:
|
Hello, you can use droop functionality for every G120. https://support.industry.siemens.com/cs/ww/en/view/12745006 -2 CU's support droop, too. Function description For mechanically coupled drives, there is the risk that the drives oppose one another: Small deviations in the speed setpoint or actual value of the coupled drives can mean that the drives are operated with significantly different torques. The droop function ensures even torque distribution between several mechanically coupled drives. The droop function reduces the speed setpoint as a function of the torque setpoint. https://support.industry.siemens.com/cs/ww/en/view/109818082 |
With best regards, |
|
6/20/2024 7:40 PM | |
Joined: 7/17/2019 Last visit: 7/8/2024 Posts: 9 Rating:
|
Thanks Technology Team, I was hoping the https://support.industry.siemens.com/cs/document/109774232/ Application can be modified for more than one slave Axis, its a tidy solution. I'll Try droop control with this Application example. It would be good if you guys made a version 2.0 for multiple Axis load sharing non mechanical coupled. FYI My 3 vector Axis are on One CU, Its actually a S120 application CU320
|
Last edited by: GChadwick at: 06/20/2024 19:43:00Thanks, |
|
6/21/2024 10:29 AM | |
Joined: 10/11/2006 Last visit: 7/12/2024 Posts: 5874 Rating:
|
Hello, if you have a CU320-2, the following drive based load sharing could be an option too: |
With best regards, |
|
Follow us on