6/26/2019 12:23 PM | |
Joined: 10/11/2006 Last visit: 9/18/2024 Posts: 5906 Rating: (804)
|
Dear Manoj R The 12 pulse rectifier circuit exist of two 6 pulse rectifiers which voltages needs being shiftet for 30°. The simpliest way doing it is by making a three winding transformer, which secondary sides connected one in Y and the other in Delta. The delta cannot be grounded sensefuly, hence the Y windings arent grounded as well. So the total system is isolated and an isolation monitoring is requred! Please find Engineering Manual SINAMICS G130, G150, S120 Chassis, S120 Cabinet Modules, S150 |
With best regards, |
|
Follow us on