10/22/2010 8:56 AM | |
Joined: 12/17/2008 Last visit: 10/26/2022 Posts: 40 Rating: (0) |
Hello I'm working on my first project with Sinaut equipment and i need your help, since i have many questions and unknown informations to solve all the problem. I have 4 pumping stations equipped with CPU 314 and TIM 3V-IE, 1 WWTP - central station were i have Master TIM 4R-IE and SCADA pc with Wincc 6.2 and ST7cc. For hardware communications i use MD741-1 GPRS Modem in pumping station and for central station Scalance S612 connected to APN . So far i made the Step 7 program for each pumping station, Wincc program for central station and communications settings for VPN tunnel between MD741-1 and Scalance 612. I use Sinaut ST7 connection configuration to manage the conections and Subscriber Administration where i chose for one pumping station from TD7 on TIM library -Bin04B_S to test the program. My questions is : What do i have to configure in ST7cc to be able to read the byte i send and generate the Wincc tag for this byte ? Any tips for how to configure the ST7cc and ST7 it will help me. Regars! AttachmentNetwork configuration.zip (126 Downloads) |
10/22/2010 2:16 PM | |
Posts: 118 Rating: (11) |
Hello Kenzo103, It is quite hard to describethis in afew lines, but the pictures in the St7cc manual are very helpful to make sure that you do everything right. You said you have written the WinCC project already? Is the ST7 channel already selected? In ST7cc you have to insert thelocalTIM (at the master side) and the stations. (You should use the right subscriber numbers as they are set in ST7) |
Follow us on