Industry Online Support
Technical Forum
8/24/2010 3:52 PM | |
Joined: 9/27/2006 Last visit: 7/14/2024 Posts: 12268 Rating: (2675) |
Hello kitec; From the Industry Mall, here is a descrition of what you have already in hand: 6ES7153-2AR03-0XA0 Now here is a description of what you want (a Y-Link to use as an interface between a redundant pair of H-controllers and single-ended Profibus slaves): The Y-Link comprises: § Two IM153-2 interface modules§ One Y-Coupler § One BM IM/IM bus module § One BM Y-Coupler bus module So you can use the IM 153-2 (-2BA02) and the IM/IM Bus module that you already have; you would need to purchase additionally the Y-Coupler and its Bus Module:Y-coupler: 6ES7197-1LB00-0XA0 Bus unit for the integration of a Y-Coupler : 6ES7654-7HY00-0XA You can check this yourself on the Siemens Industry Mall: https://eb.automation.siemens.com/goos/WelcomePage.aspx?regionUrl=/UK&language=en You could also confirm the information in the manual for the Y-Link: http://support.automation.siemens.com/WW/view/en/1142696 Daniel Chartier |
Last edited by: dchartier at: 8/24/2010 3:54 PM |
|
8/25/2010 6:54 AM | |
Posts: 10 Rating: (0) |
Dear Daniel Chartier, Thanks a lot for your prompt reply. It solved the problem. Best Regards, Kitec. |
Follow us on