10/14/2021 9:43 AM | |
Posts: 4 Rating:
|
I would like to return to the topic of the SIEMENS 3M controller ... I have a problem with starting the machine after replacing the memory backup battery. After performing the RESET procedure on the 03840 board, two red LEDs are on, even though the 3M controller is green. In general, the 3M controller is very picky when it comes to the RESET procedure because I manage to turn on the green LED in the steron for 20-30 attempts, only after one more the LED change from red to green - but on the 03840 board the left red diode stops flashing and lights up permanently - i.e. two red LEDs are still on. I am asking for help, because maybe they will wrongly carry out the RESET procedure... I do that: 1 - I put the RUN / STOP switch on the 3M controller to the STOP position. 2 - I press and hold three switches - two on the 3M controller Reset and Restert + Reset switch on the power supply. 3 - I release all three switches and set RUN / STOP to RUN position and press Reset on the power supply again. I do all this procedure smoothly with one-second breaks - what am I doing wrong ??? that I fail to pick up the system ??? I also have a question in what position the switch on the upper part of the 03840 board should be at the time of the RESET procedure ??? ------------------------------------------------------------------------------------------ |
Last edited by: Rumet at: 10/14/2021 10:00:53Last edited by: Jen_Moderator at: 10/14/2021 11:19:09New subject after splitting |
|
10/14/2021 10:00 AM | |
Posts: 4 Rating:
|
I will add a photo with a switch on the 03840 board |
Follow us on