6/20/2012 10:42 AM | |
Posts: 5 Rating:
|
Hi. I have an erased Sinumerik 810 GA1 and I need to reload all files (TEA1, TEA2 and PCP). I have all of them, but the PLC file I have is in S5D format and unfortunetly the PLC connection with Step5 program doesn't work with this GA1 since something wrong is with its PLC interface. I need a favour from someone who have a working Sinumerik 810 GA1 to upload an attached S5D file to his GA1 and then download it via V24 in %PCP format. I'm trying to do that with GA2 and GA3, but then I can't download the PCP file to GA1. Best regards, Miro AttachmentPLC435ST.zip (357 Downloads) |
Last edited by: miroksp at: 6/20/2012 10:42 AM |
|
6/20/2012 4:45 PM | |
Posts: 2964 Rating:
|
Hello... If you have your PCP try loading it....getting any error Check this link for downloading: /tf/WW/en/Posts/50916 Regards, Prakash |
6/21/2012 9:24 PM | |
Joined: 7/16/2006 Last visit: 7/27/2023 Posts: 1502 Rating:
|
Hi X121 --> V24 and TTY boot is posible for read in. I mean using for Step 5. Urgent: Make sure, that the V24-Cable is lower the 5 meter. ( inch ? ) Here is the Book_820_with information See Page 125 Capter 7-11 Please Try this. Regards Karl |
Karl |
|
This contribution was helpful to
1 thankful Users |
6/29/2012 9:55 AM | |
Posts: 5 Rating:
|
I've solved the problem with RS232/current loop converter: http://datainterfaces.com/usermanual/ICCL-2-manual.pdf Regards, Miroslav Attachment227_800 Universal Interface Planning Guide.pdf (368 Downloads) |
This contribution was helpful to
2 thankful Users |
Follow us on