11/3/2020 12:24 PM | |
Joined: 3/2/2007 Last visit: 9/17/2024 Posts: 935 Rating: (5) |
Kindly, which Sitop is most suitable, for 24vdc supply of, ET200SP modules and Sinamics S120 drives? We need it with 220 vac input and 24vdc 20A output. 6EP1336-3BA10 , SITOP PSU8200 20 A Stabilized power supply input: 120-230 V AC 110-220 V DC output: 24 V DC/20 A 6EP1336-2BA10 , SITOP PSU100S 20 A Stabilized power supply input: 120/230 V AC, output: 24 V DC/20 A 6EP1336-1LB00 , SITOP PSU100L 24 V/20 A Stabilized power supply input: 100-240 V AC output: 24 V DC/20 A |
... thank you ... |
|
11/3/2020 3:57 PM | |
Joined: 9/27/2006 Last visit: 9/18/2024 Posts: 12282 Rating: (2684) |
Hello Ziemens; Have a look at the S120 AC drive manual, this section covers 24 VDC power supply recommendations: There is only one that fits all your stated requirements. https://support.industry.siemens.com/cs/ww/en/view/99673000/64061212683 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 11/03/2020 16:23:21 |
|
11/3/2020 4:10 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello, 6EP1336-3BA10 |
Last edited by: Ste39 at: 11/03/2020 16:49:27Last edited by: Ste39 at: 11/03/2020 16:50:10after correction of our Expert dChartier |
|
This contribution was helpful to1 thankful Users |
11/3/2020 4:47 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello daniel, great, why don't they update them |
This contribution was helpful to1 thankful Users |
11/4/2020 3:00 PM | |
Joined: 3/2/2007 Last visit: 9/17/2024 Posts: 935 Rating: (5) |
Kindly, we are using the 6EP1336-2BA10 , is it close enough to the 6EP1336-3BA10 supply ? |
... thank you ... |
|
11/4/2020 4:35 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello, yes is the same, no have only the VDC input |
11/4/2020 5:01 PM | |
Joined: 9/27/2006 Last visit: 9/18/2024 Posts: 12282 Rating: (2684) |
Hello Ziemens; The specs of the 2 units are similar as Ste39 has pointed out, but there are important differences in startup and overload protections provided by the 2 families of power supplies, PSU8200 and PSU100S. It would be best if you looked at their technical data, along with this presentation of the Sitop family, and choose based on the performance and protection you need in this situation, and not only for price. Only you can decide what is best for your project. SITOP Power Supply. Brochure incl. technical data https://support.industry.siemens.com/cs/ww/en/view/109765864 6EP1336-2BA10 :SITOP PSU100S/1AC/24VDC/20A https://support.industry.siemens.com/cs/pd/308553?pdti=td&dl=en&lc=en-WW 6EP1336-3BA10:SITOP PSU8200/1ACDC/24VDC/20A https://support.industry.siemens.com/cs/pd/385111?pdti=td&dl=en&lc=en-WW Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 11/04/2020 17:03:15 |
|
Follow us on