6/19/2014 5:09 PM | |||
Joined: 9/27/2006 Last visit: 8/13/2024 Posts: 12277 Rating: (2680) |
Hello Will; Did you really meana Sitrans LU250 HART, or did you mean a Sitrans LU250 Profibus-PA? If you want to use HART communications, you would need the following HART input module, and it can only be mounted on a Profibus-DP slave station (ET 200M):
If you do intend to use Profibus-PA in your project, please look at the recent thread giving abasic overview on connecting PA instruments to a DP-master: In the meantime you could look at the manuals for both types of intrument, so you can see the differences between the two (as far as communications with the PLC): SITRANS LR250 (HART) - Operating Instructions SITRANS LR250 (PROFIBUS PA) - Instruction Manual Hope this helps, Daniel Chartier |
||
6/19/2014 10:26 PM | |
Posts: 2 Rating: (0) |
thanks sir, very helpful info |
6/24/2014 9:55 AM | |
Joined: 12/13/2012 Last visit: 10/5/2023 Posts: 124 Rating: (45)
|
For the Profibus PA versions, there is also a application guide in the internet. Maybe this is also helpfull for you. Here the link ==> http://www.automation.siemens.com/mcms/sensor-systems/SiteCollectionDocuments/pi/application_guides/en/AG060417.pdf Cheers Levelmans |
This contribution was helpful to1 thankful Users |
Follow us on