8/10/2016 2:11 PM | |
Joined: 3/11/2007 Last visit: 7/18/2024 Posts: 226 Rating: (13) |
Hello, For the first time using this product: Sitrans Probe LU. I read that you can program it via HART protocol. I own a programming console from another device. http://www2.emersonprocess.com/siteadmincenter/pm%20rosemount%20documents/00809-8020-0001.pdf I was wondering if this console could also be used on the Probe LU. I'm not familiar about. Thank you
|
8/10/2016 2:34 PM | |
Joined: 9/27/2006 Last visit: 9/15/2024 Posts: 12282 Rating: (2683) |
Hello automatizzando; Here is the manual for the Sitrans Probe LU, with HART protocol: SITRANS Probe LU (mA/HART) - Operating Instructions https://support.industry.siemens.com/cs/fr/en/view/109482629 Siemens offers a handheld HART communicator for the Sitrans Probe LU, it uses IR communications with the instrument. I am not sure whether a 3rd-party communicatorcan easily be used for programming th unit. I suggest tou open a Support Request and ask Siemens techs if you can connect with your specific HART communicator to the Sitrans Probe LU unit to change parameters. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 8/11/2016 2:22:40 PM |
|
8/11/2016 10:17 AM | |
Joined: 12/13/2012 Last visit: 10/5/2023 Posts: 124 Rating: (45)
|
Hi , you can use a HART Communicator 275/375 for the programming of the Probe LU. Please find the DD attached. Additional., you also can use Simatic PDM to program the Probe LU via HART. Hope this helps ! Attachmentdd.zip (166 Downloads) |
Last edited by: Levelmans at: 8/11/2016 10:18:39 AM |
|
This contribution was helpful to1 thankful Users |
8/24/2016 10:56 AM | |
Posts: 6 Rating: (2) |
Was most helpful for me ! Thanks ! |
8/24/2016 11:22 AM | |
Joined: 12/13/2012 Last visit: 10/5/2023 Posts: 124 Rating: (45)
|
Thanks for the feedback! |
Follow us on