1/24/2018 11:28 PM | |
Posts: 18 Rating: (0) |
I setup a TP900 Comfort back in February of 2017 for Remote Access using the Sm@rtClient App. Everything worked great until around October. When my customer uses the Sm@rtClient App a gray screen is displayed with the "No Input" icon. I originally figured that it had something to do with IOS 11. I had an associate install the Sm@rtClient Lite App on an IPhone with IOS 10.1.2 and the app worked great. I had another associate install the same app on IOS 11.2.1 and the app worked as well. I get the same gray screen and icon on my IPhone with IOS 11.2.2 that previously worked. I had hoped that the most recent app update on 01/22 would resolve the problem but no luck. I have performed a hard reset of my IPhone and reset my network settings back to default without any success. I have contacted tech support but they can not duplicate the issue. I would greatly appreciate any suggestions. My customer is really getting frustrated that they can no longer access their system. |
1/25/2018 6:13 PM | |
Posts: 18 Rating: (0) |
Thank you fro the suggestion. I have updated to the current app and I still have the same issue. What would be the next step? |
8/16/2019 6:43 PM | |
Posts: 1 Rating: (0) |
Hi, I have the exact same issues, tried update but still have the grey screen, has anyone else come across this? |
4/12/2022 3:54 PM | |
Joined: 1/13/2020 Last visit: 7/8/2024 Posts: 11 Rating: (0) |
Happened to me when I accidently set the Visibility animation to the whole main screen instead of an element on it. |
6/24/2022 5:50 AM | |
Joined: 6/19/2017 Last visit: 6/28/2024 Posts: 8176 Rating: (169) |
New question published by Zivelion is split to a separate thread with the subject "No Input" Icon. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on